Devices
Use Devices to add one or more devices from your system into the project.
To add one or more devices to your project:
- Select either:
- Import Devices From CSV and then use Manage Multiple Devices to import multiple devices. For more information,, see Define multiple devices using a CSV file
OR
- Manage a Single Device and then create the device using the I/O Device Manager. For more information,, see Define one I/O device in a project.
- Import Devices From CSV and then use Manage Multiple Devices to import multiple devices. For more information,, see Define multiple devices using a CSV file
- Select Next.
For more information on Power Operation device configuration, see Manage I/O devices in a project.