Plan

Power Operation is uniquely designed to let you take advantage the power of a SCADA for Power Management Applications.

Power Operation with Advanced Reporting and Dashboards enables the Facilities Team in Power Critical Facilities to monitor, control, and troubleshoot issues in real-time with their electrical distribution systems.

Use the information provided in this section to prepare for an installation or upgrade of a Power Operation system.

Use the links in the following table to find the content you are looking for:

Topic Content
Components and single-site architectures Information on design considerations for components and component architectures.
Multi-site architectures Discusses scaling your system with multi-site architectures.
Connected devices and protocols Information on Power Operation's support for concurrent protocol communication.
Computer requirements Information on hardware and software requirements for Power Operation.
Web Client versus Thick Client Discusses the web client features compared to the thick client features.
Translation Information on which languages Power Operation components are localized.
Commercial references Lists commercial references.
Integrating with Advanced Reporting and Dashboards Information on integrating with the Advanced Reporting and Dashboards module.
Interoperability Provides information on integrating Power Operation with other systems.
Power SCADA Anywhere Provides details on the Power SCADA Anywhere component and architectures.
OFS system time stamping Provides information on time stamping and related topics.