Configure the Power Operation Secondary Server
NOTE: This section assumes that the Power Operation project and the Primary Server are configured,
Complete the following tasks to configure the Power Operation Secondary Server:
- Restore the Power Operation Studio project
- Import the One-Time Password
- Import the Advanced One-Line Encryption (AES) File
- In the Application Configuration Utility:
- Re-enter SSO passwords in . For more information,, see Configure Single Sign-On (SSO).
- Re-enter the Citect Data Platform password. For more information,, see Set up data acquisition parameters.
- Add INI edits to the standby server
citect.inifile. Other settings from the primary server citect.ini file, such as I/O device parameters and any other customizations, will need to be added to the standby servercitect.inifile. - Configure the notifications. See Notifications in a redundant system for details.