Installing Cybersecurity Admin Expert
Cybersecurity Admin Expert (CAE) does not install with Power Operation, and must be downloaded and installed independently.
NOTE: If you have an existing CAE project, create a backup before installing Power Operation.
CAE installation requirements:
- Power Operation installed.
- Refer to the CAE User Guide for operating system requirements.
- Download and extract Cybersecurity Admin Expert ZIP file.
- ZIP file x86 for Windows 32-bit systems.
- ZIP file x64 for Windows 64-bit systems.
- Other software components automatically installed in order to properly run CAE. For more information, see System software order of installation.
- Windows Administrator username and password credentials.
notice
data LOSS
Back up your Cybersecurity Admin Expert project and other relevant historical data files from all servers in the system prior to installing Power Operation.
Failure to follow these instructions can result in a loss of data.
To install CAE:
- If you have an existing CAE project:
- Delete the certificate in the current CAE.
- Rediscover the devices.
- Click Send the security configuration to send the configuration from CAE to Power Operation.
- Right-click the Cybersecurity Admin Expert ZIP file, and then select Extract All... > Extract.
- Double-click the EXE file. The Cybersecurity Admin Expert wizard opens.
- Select the language, and then click OK.
- Click Install.
- Click Next to go through the screens and select the options you want.
- Click Install.
- Click Finish. Cybersecurity Admin Expert icon is created on the desktop.
For detailed steps on configuring CAE, see Configuring CAE cybersecurity.