Cybersecurity Checklist
Cybersecurity configuration checklist
| Action | Link |
|---|---|
|
Address potential risks using compensating controls. |
Potential risks and compensating controls |
| Set-up user access and apply least privilege. | |
|
Harden environments, change port numbers from default values, and configure server and firewalls to restrict and control traffic between IT, OT, and Internet network zones. |
|
| Follow allowlisting design considerations and use application allowlisting and McAfee to prevent unauthorized applications from running on your systems. | |
| Configure the Service Layer, set permissions on the certificate, and update the registry configuring third-party certificates. | Configuring third-party certificates |
| Configure a one-time password for two-factor authentication using a YubiKey USB key device. | Configuring two-factor authentication |
| Configure to communicate with multiple network adapters in a segmented architecture. | Configuring projects for network segmentation |
See Using Cybersecurity Admin Expert (CAE) for cybersecurity for information on configuring cybersecurity using the CAE tool.
See Decommission for recommendations and procedures about decommissioning.
See:
- Product defense-in-depth for details about defense controls in your IT and control system to maximize data protection.
- Cybersecurity capabilities for more details about information confidentiality.