Adding Paths

When you create a path of one or several objects, you create a copy in the form of a path, where the original objects have been dissolved and replaced with corresponding lines and fills. For example, a rectangle dissolves into a path of four connected strokes.

By creating a path, the number of objects is reduced to one. That is, the resulting path.

The advantage of using a path is that it speeds up the drawing of the object, which can be important when using animations.

The original objects remain unchanged and can be deleted, if required.

For more information, see the following sections: