TGML Animations

An animation is a time-based modification of an element attribute. The animation defines a mapping of time to values for the target attribute.

The TGML implementation (Graphics Services) only runs animations in Dynamic mode. The value of an attribute that has been animated (changed) in Dynamic mode is not preserved in the TGML file. The animated value is only valid while running in Dynamic mode.