Operate
Use the information provided in this section to use the Power Operation runtime.
Use the links in the following table to find the content you are looking for:
| Topic | Content | 
|---|---|
| Infomation on login procedures. | |
| Interface overview | An overview of the Power Operation Runtime interface. | 
| Viewing Alarms and Events | Information on operating Alarms and Events. | 
| Analysis Page | How to use the Analysis Page to view trend data. | 
| Equipment Pop-Up Page | How to use the Equipment pop up page to see the detailed status of a particular device and to control the device. | 
| IEC 61850 advanced control | How to access the advanced control window. | 
| Tag Viewer | Customizing advanced reports and design considerations for device communication in Power SCADA Operation with Advanced Reporting and Dashboards. | 
| Basic Reports | Information on the Power Operation basic reports. | 
| Web Applications | How to use Alarms, Diagrams, and Trends. | 
For more detailed resources on operating, see the Operate references section.