Configuring Power Measurement components to monitor electrical health

Use the Power Measurement Display Bar with the Power Measurement Selector to display real-time values that indicate the health of your electrical system. For more information, see Electrical Health TGML components.

To configure Power Measurement components:

  1. In Graphics Editor, from the Components pane > Power Measurement category, drag the Power Measurement Display Bar and Power Measurement Selector to the work area.
  2. In the Objects pane, bind your equipment to the Power Measurement Display Bar.
  3. In the Properties pane, for each measurement, set the following to match the equipment’s operational ranges:
    • Item name.
    • The minimum and maximum values.
    • Appropriate setpoint values.

    You can now use the Power Measurement Selector drop-down to select the electrical parameters to measure and display. Options include:

    • Voltage
    • Current
    • Active power
    • Power factor