When the EcoStruxure Machine Expert Twin layout is set to default mode, you will find the Solution Explorer and Statistics window on the top right side of the screen. This window has a few different functions:
Solution Explorer
The solution explorer contains a three structure that lets you see every assembly you have placed onto the model floor. It has three different categories: assemblies, motors and controllers. Assemblies is sorted into sections which then shows each assembly that section contains. In the solution explorer you can get a quick overview of every single thing, you have placed. If you click on any of them, the model will highlight that assembly for you. You can move assemblies between different sections by dragging them into another section tab or by choosing the assembly you want to move and then changing the section it is placed under in the properties window. You can rename sections by clicking on the section and then change the name in the properties window.
If you right click on the assemblies tab, you will see a menu that looks like this:
In the menu you can choose to add a section or show all sections. You can also Collapse All which will close all the subcategories you have open. If you right click on the motors tab, you will also be able to collapse all. Right clicking on the controllers tabs will open a menu which says ‘Load’. Here you can load a controller file (.DLL format) into EcoStruxure Machine Expert Twin. When the controller is loaded it shows up in the solution explorer window like this:
If you open the assemblies menu and right click on the sections you will see a new menu:
HIDE ALL SECTIONS BUT THIS: See only this section
SHOW ALL SECTIONS: See all the sections again
HIDE ASSEMBLIES: Hides all assemblies as well as the floor of that section
LOCK ASSEMBLIES: Locks every assembly you have placed up to that point but does not not lock new assemblies you place
FIT: Resizes the floor to fit around the assemblies placed in the model
DELETE (Name): Delete the chosen section. It is not possible to delete the last section to have no sections
DISABLE ASSEMBLIES: When you disable the assemblies of a section all the assemblies placed in that section will turn gray to show they are disabled. When you for example place a load on a disabled assembly it will fall trough the assembly.
COLLAPSE ALL: Collapses the tree hierarchy
If you right click on one of the assemblies in the assemblies tab, you will have the choice to either disable the assembly or delete it. If you right click on a motor you will have the choices to start the motor, copy it, disable it or delete it.
The solution explorer window also has a few more options to individualize the window. In the right corner you will see a small tack which will allow you to ‘auto hide’ the window. Pressing this will place the window as a bar just below the EcoStruxure Machine Expert Twin menu like this:
To reset it go to the View menu and press reset. Below the tack is a search bar where you can search for any assembly or motor you have placed on the model floor and next to that is a button with three lines that will let you choose whether or not you want to see the assemblies assorted into categories.
Statistics
The statistics window displays information about the loads in the model:
You can get information from a specific sensor by adding it to the statistics window. To do this you right click on the sensor you want to display and choose ‘Observe’. Now the sensor shows up in the statistics display under the Loads line:
You can observe different types of sensors, scanners, weights, counters and eaters. The scanners will show information about how many loads they have scanned, while the buttons show how many times they have been pressed.
If you want to change the name of any of the sensors just click on the sensor in the model and its information will show up in the properties window. From here you can change the name. To display the new name simply right click the sensor, uncheck ‘Observe’ and check it again. Now the sensor should show up in the statistics window with its new name.