Performance Tips

Power Settings

  • Disable all power saving modes.
  • Set Power Options to maximum performance
  • Note that domain rules affect this
  • While using Machine Expert Twin (MET) dongles, any power loss on usb will result in MET closing

Labels (2D Graphic)

  • Adding a large amount of “external” graphic, using labels, enabling of assembly text or similar can dramatically decrease performance. As movable objects, each one is rendered separately.
  • Using lots of this on a large model on pc with limited capability equals low performance

Increase Performance

  • Improve performance by disabling shadows, lowering antialiasing, or setting detail level to “Normal” or “Primitives”.
  • Settings can be found in the Pane “View” under section “Visibility”.
  • Close windows you do not need. Especially closing the Solution Explorer in model with thousands of assemblies can help quite a bit.
  • Window layout can be reset, or single window added, if later needed
Next InfluxDBLogTarget