RFC1006 – Protocol

The EcoStruxure Machine Expert Twin implementation of the RFC1006 protocol is not the full implementation specified in the public RFC1006 protocol specification.

We have focused on creating a simple and reliable communication protocol and the implementation has primarily been developed in order to meet the Siemens SIMATIC PLC requirements.

The RFC1006 protocol is designated ISOonTCP in a Siemens PLC. Note that the protocol specified in this manual is implemented in full by Siemens PLC network card, i.e. no user program necessary to implement this protocol.

Properties

  • Identification
    • Name – Customizable name
    • Id – Customizable Id
  • Communication
    • Port Number – Port used for communication between EcoStruxure Machine Expert Twin and “Device”
    • IP Address – Type in IP address (only available if Mode = Client)
    • Mode – Select “Server” or “Client”
    • Auto Connect – Activate or Deactivate whether EcoStruxure Machine Expert Twin should try to automatically connect to the “Device”
    • Auto Connect Delay – Set delay for when the connection will try to reconnect
  • RFC1006
    • Remote TSAP – Address of Remote TSAP (Transport Service Access Point)
    • Local TSAP – Address of Local TSAP (Transport Service Access Point)
    • Connection Id – Connection Id used
    • Max TPDU Size – TPDU (Transport Protocol Data Units) maximum size
    • Max TPDU Bytes – TPDU (Transport Protocol Data Units) maximum bytes used
    • Send Connection Request – Activate or Deactivate whether or not a connection request is to be sent
    • Sign Of Life – Activate or Deactivate whether or not Sign Of Life signal is to be used
    • Sign Of Life Interval – Set the time interval between Sign Of Life requests (only Available if Sign Of Life is checked)
    • Sign Of Life Timeout – Set the timeout value (only Available if Sign Of Life is checked)
Previous 3964R-Protocol