|
Step |
Action |
|---|---|
|
1 |
After starting the installer, the Select a Task dialog is displayed. |
|
2 |
Select the option Modify Installed Software. |
|
3 |
In the Select Product section, select the following options: oProduct: Select your installed product. oVersion: Select the version of your installed product. |
|
4 |
In the Choose an action section, select Add-Ons/Patches. |
|
5 |
Select Source: Online and click Next. NOTE: You can also use one of the other two options, but if there is an Internet connection available, the preferred Source is Online to download and install the software directly from the Schneider Electric server. |
|
6 |
Click Next and browse for the Add-Ons or Patches. |
|
7 |
From the list of Components, select an Add-On or Patch you wish to install. |
|
8 |
Click the Start Installation/Uninstallation button. |