|
Type: |
Enumeration |
|
Available as of: |
V1.0.0.0 |
The enumeration ET_Result contains the possible values that indicate the result of operations executed by the function block.
|
Name |
Data type |
Value |
Description |
|---|---|---|---|
|
If q_xError of a function block is FALSE, the following status message is shown. |
|||
|
DINT |
0 |
Operation completed successfully. |
|
|
If q_xError of a function block is TRUE, one of the following status messages is shown. |
|||
|
DINT |
1 |
The TCP operation was not completed successfully. General TCP issue, refer to the TcpUdpCommunication Library Guide. |
|
|
DINT |
26 |
The given IP address is not valid. Verify the setting of the iq_stConnSettings.wsGpIpAddress input. |
|
|
DINT |
28 |
The client is not connected to the TCP server. Verify that the SQL Gateway is installed and running within the specified IP address and port. |
|
|
DINT |
41 |
Remote system is not available or is not answering the request. Verify that the SQL Gateway is installed and running within the specified IP address and port. |
|
|
DINT |
61 |
DbConnectionName is empty (Null). Element wsDbConnectionName from input iq_stConnSettings is blank. |
|
|
DINT |
63 |
User buffer is insufficient for returning data. Matching the returning numbers of rows and columns with the settings in the global parameter list, you can find the minimum settings at q_uiRetNumOfRows (q_uiRetNumOfColumns) of FB_SqlDbRead after each execution. |
|
|
DINT |
64 |
A former request is currently being processed. Another instance with the same input for iq_stConnSettings is currently executed (output q_xBusy = TRUE). |
|
|
DINT |
65 |
Controller received an invalid message from the SQL Gateway. Contact your local Schneider Electric support. |
|
|
DINT |
66 |
Function block operation timeout expired. Verify the setting of the input iq_stConnSettings.timSqlTimeout depending on the system configuration the default value must be increased. |
|
|
DINT |
67 |
Transaction number mismatch. Contact your local Schneider Electric support. |
|
|
DINT |
68 |
Transmission number mismatch. Contact your local Schneider Electric support. |
|
|
DINT |
69 |
TcpUdp client connection already occupied with another service.Verify that no other instance of TCPUDP.FB_TCPClient inside your application occupies the connection. |
|
|
DINT |
70 |
Method Shutdown or Close from TcpUdp client not successful. TCP connection issue. Restart your controller. |
|
|
DINT |
71 |
The function block FB_SqlDbGetData does not provide any data. The SQL request was executed successfully but no data returned. Verify that the assigned database contains data. |
|
|
DINT |
72 |
TcpUdp client system is not ready to receive or transmit data. TCP connection issue. Restart your controller. |
|
|
DINT |
80 |
The given port number is equal to zero. Verify the iq_stConnSettings.wGwPort input. Usually, the default value 3457 is used. |
|
|
DINT |
81 |
The input i_uiNumOfWstrings is less than 1 or greater than GPL.Gc_uiMaxRequest. Verify the i_uiNumOfWstrings input. At least one WSTRING is required. Also verify that the given number is greater than the limit GPL.Gc_uiMaxRequest (GPL). |
|
|
DINT |
82 |
Empty request string or invalid reference (NULL). Verify the i_refRequestWstring input. The first WSTRING (i_refRequestWstring[1]) must contain any character. Verify that if the input is assigned. |
|
|
DINT |
83 |
Invalid user data reference (NULL). Verify that the i_refUserData input is assigned. |
|
|
DINT |
85 |
GPL.Gc_uiMaxRows is out of range. Verify the settings of Global Parameter List. |
|
|
DINT |
86 |
GPL.Gc_uiMaxColumns is out of range. Verify the settings of Global Parameter List. |
|
|
DINT |
87 |
GPL.Gc_uiTableWstringLength is out of range. Verify the settings of Global Parameter List. |
|
|
DINT |
88 |
GPL.Gc_uiRequestWstringLength is out of range. Verify the settings of Global Parameter List. |
|
|
DINT |
89 |
GPL.Gc_uiMaxRequest is out of range. Verify the settings of Global Parameter List. |
|
|
DINT |
91 |
GPL.Gc_uiRecBufferLength is out of range. Verify the settings of Global Parameter List. |
|
|
DINT |
92 |
GPL.Gc_uiSendBufferLength is out of range. Verify the settings of Global Parameter List. |
|
|
DINT |
100 |
SQL Gateway connection name does not exist. Verify available database connections from SQL Gateway console. |
|
|
DINT |
101 |
SQL Gateway connection configuration does not match. Execute Test Database Connection from SQL Gateway console. |
|
|
DINT |
102 |
SQL Gateway connection to the database does not work. Execute Test Database Connection from SQL Gateway console. |
|
|
DINT |
120 |
Protocol error between SQL library and gateway detected. Contact your local Schneider Electric support. |
|
|
DINT |
150 |
Execution of the SQL request not successful. Verify i_refRequestWString input according to the required SQL syntax. Refer to SQL server manual. |
|
|
DINT |
151 |
SQL Gateway does not provide an answer. Verify that the addressed database contains any data with an additional application. |
|
|
DINT |
170 |
SQL Gateway license issue. Open the License Manager to verify that SQL for EcoStruxure Machine Expert is valid. |
|
|
DINT |
199 |
SQL Gateway error detected. Contact your local Schneider Electric support. |
|
NOTE: The results in the range 100...199 are messages from SQL Gateway. Refer to SQL Gateway User Guide.
oFB_SqlDbRead
oFB_SqlDbWrite