Project Archives Helping to Preserve Compatibility
Before you install a new version of EcoStruxure Machine Expert software, or when your project is completed, it is a good practice to create an archive of your project. The archive contains all files included and referenced in the project with settings and profiles.
Project archives provide the following advantages:
oYou can extract the project archive to any computer with EcoStruxure Machine Expert installed. In this way, you can share your projects with others or run it on another computer.
oCreating an archive can help reduce compatibility concerns with later versions of EcoStruxure Machine Expert.
This chapter provides information on the specific settings that help to preserve compatibility.
For information on creating project archives, refer to the description of the File > Project Archive > Save/Send Archive... command in the EcoStruxure Machine Expert Menu Commands Online Help.
NOTE: Obsolete devices that are not supported by the present EcoStruxure Machine Expert software are not installed on the local system and are therefore not available in the Device Repository dialog box.
Settings Helping to Preserve Compatibility
When you create an archive on your local computer by executing the File > Project Archive > Save/Send Archive... command, the Project Archive dialog box opens.
In the Project Archive dialog box, the following topics can affect compatibility and therefore you can select them when appropriate:
Information |
Description |
---|---|
Download information files |
When this is selected, the compile information (the *.compileinfo file) is saved with your project file. This allows you to log in to the controllers with the archived project without rebuilding the project. |
Referenced devices |
When this is selected, the devices in the Device Repository of your project are saved into the archive with their versions. Devices installed with EDS files are included. |
Referenced libraries |
When this is selected, the libraries in the Library Repository of your project are saved into the archive with their versions. Third-party libraries are included. |