Malfunction |
Probable cause |
Solution |
---|---|---|
Trouble with components. |
End of component life cycle. |
Note the maintenance plan. |
Squeaking. |
Ball sockets are contaminated. |
|
Ball sockets are worn out. |
||
Ball bearing at parallel pate is contaminated. |
||
Spring roll is worn out. |
||
Rattling noise. |
A spring is absent and/or damaged. NOTE: Verify the upper arm regarding mechanical attachment. |
|
Oil beads up at new gearbox. |
Initial oozing of new gearboxes. |
|
Grease at new ball bearing. |
Initial oozing of new bearings. |
|
Extensive position deviation after motor replacement. |
The robot is not calibrated. |
|
Incorrect motor replacement. |
||
Rotational axis has backlash. |
Rotational axis is worn out. |
Verify and replace if necessary. |