IF_RobotFeedbackTracking - General Information
Type: |
Interface |
Available as of: |
V1.6.0.0 |
Inherits from: |
- |
This chapter provides information on:
oTask
Interface with return values of a tracking movement of the robot.
In case of an active tracking movement in a configured linear tracking system configured by IF_RobotConfiguration.AddLinearTrackingSystem, the feedback values are provided within this feedback interface.
Name |
Data type |
Accessing |
Description |
---|---|---|---|
etPhase |
Read |
Phase of a tracking movement. |
|
lrOffsetAccelerationResultant |
LREAL |
Read |
Resultant offset acceleration of a tracking movement. |
lrOffsetPositionResultant |
LREAL |
Read |
Resultant offset position of a tracking movement. |
lrOffsetVelocityResultant |
LREAL |
Read |
Resultant offset velocity of a tracking movement. |
lrRemainingTime |
LREAL |
Read |
Remaining time until the tracking synchronization phase is finished. Unit: [msec] |
lrRemainingTimePathPositionEnd |
LREAL |
Read |
Remaining time until the specified end position on path of the tracking synchronization phase is reached. The value 0.0 is returned if the tracking synchronization phase is not started or changing the coordinate system was not requested by a call of the method IF_RobotMotion.ChangeCoordinateSystem2(…). Also refer to Behavior of IF_RobotFeedbackTracking.lrRemainingTimePathPositionEnd. |
rstEstimatedStopPosition |
REFERENCE TO PDL.ST_Vector3D |
Read |
Estimated Cartesian stop position where an active tracking is stopped. For example, with FB_Robot.xEnable TRUE -> FALSE or in other emergency stop situations (refer to Behavior of feedback property rstEstimatedStopPosition). |
rstOffsetAcceleration |
REFERENCE TO PDL.ST_Vector3D |
Read |
Offset acceleration of a tracking movement in cartesian coordinates in relation to the robot coordinate system ET_CoordinateSystem.CSR. |
rstOffsetPosition |
REFERENCE TO PDL.ST_Vector3D |
Read |
Offset position of a tracking movement in cartesian coordinates in relation to the robot coordinate system ET_CoordinateSystem.CSR. |
rstOffsetVelocity |
REFERENCE TO PDL.ST_Vector3D |
Read |
Offset velocity of a tracking movement in cartesian coordinates in relation to the robot coordinate system ET_CoordinateSystem.CSR. |