The SF_ESPE function block monitors the switching states of electro-sensitive protective equipment (e.g., a light curtain or light grid) and executes stop category 0 at its output. S_StartReset and S_AutoReset can be used to specify a start-up inhibit and a restart inhibit.
This documentation refers to the electro-sensitive protective equipment as ESPE for short.
When the connected ESPE triggers, the function block ensures that the enable signal at the S_ESPE_Out output switches to SAFEFALSE. The process being controlled is stopped.
S_StartReset is used to specify the start-up inhibit after activating the function block and/or starting the Safety Logic Controller.
|
S_StartReset = SAFEFALSE |
After the Safety Logic Controller has been started up and/or the function block has been activated at input Activate, the start-up inhibit is active. The start-up inhibit is only removed if there is a positive signal edge at the Reset input. Refer to the hazard message below this table. |
|
S_StartReset = SAFETRUE |
After the Safety Logic Controller has been started up and/or the function block has been activated at input Activate, no start-up inhibit is active. Refer to the section "Attention when using ...". |
Removing the start-up inhibit by means of a positive signal edge at the Reset input can cause the S_ESPE_Out output to switch to SAFETRUE immediately (depending on the status of the other inputs).
| WARNING | |
|---|---|
S_AutoReset is used to specify the restart inhibit that is active when the connected ESPE that was previously triggered is no longer triggered (as the light curtain or light grid, for example, is no longer interrupted).
|
S_AutoReset = SAFEFALSE |
Once the ESPE that was previously triggered is no longer triggered, the restart inhibit becomes active. The restart inhibit is only removed if there is a positive signal edge at the Reset input. After the restart inhibit has been removed, the status at the S_ESPE_Out output can switch from SAFEFALSE to SAFETRUE. Refer to the hazard message below this table. |
|
S_AutoReset = SAFETRUE |
The restart inhibit is not specified. As soon as the ESPE that was previously triggered is no longer triggered, and the value SAFETRUE is present at the S_ESPE_In input again, the S_ESPE_Out output automatically switches to SAFETRUE. Refer to the section "Attention when using ...". |
Removing the restart inhibit by means of a positive signal edge at the Reset input can cause the S_ESPE_Out output to switch to SAFETRUE immediately (depending on the status of the other inputs).
| WARNING | |
|---|---|
The start-up inhibit and/or restart inhibit must only be deactivated if it is certain that starting up/restarting the machine/system will not lead to a hazardous situation or that a suitable start-up/restart inhibit is in place at another location or using other means.
| WARNING | |
|---|---|