TYPE SMC_GCODEVIEWER_DATA : STRUCT
An array of this structure is used as data buffer by the FB SMC_GCodeViewer; one variable of this type stores one line of a G-code file.
Name
Type
Initial
Comment
wGCodeViewertructID
WORD
16#6911
Internal ID
iLine
DINT
Line number
str
STRING
G-code line as string