FUNCTION_BLOCK SMC_GCodeViewer
This function block produces a textual representation of the G-Code that has been processed by SMC_NCInterpreter or SMC_NCDecoder. This textual representation can be displayed in a visualization. With the input iActObjectSourceNo, typically connected with the SMC_Interpolator output iActObjectSourceNo, the function block gets the information which line has already been processed. It will remove the text of already processed lines.
The output of the function block does not exactly match the G-code stored in the editor or in the text file. For example, no blank lines or comments will be output and variables will be replaced with their value.
The function block is called in the same task as SMC_NCInterpreter.
The number of SMC_GCODEVIEWER_DATA objects in the buffer pBuffer must be at least as large as the sum of all SMC_GEOINFO objects which are can be stored in the buffers of the SMC_NCInterpreter and the path-preprocessing function blocks.
| InOut: |
|