Command 'UpdateToHeadRevision'

Function: Updates the CODESYS project with the changes from the SVN repository.

Call: Action in the Test Manager TestManager.SVN

Requirement: The CODESYS Test Manager add-on is installed.

See also