Command 'Update only this'

Symbol:

Function: The command updates the selected objects. In contrast to the Update and Update to Revision commands, the child objects are not updated.

Call: Context menu ‣ SVN

See also