Library: IODrvEtherCAT
Like ETC_CO_SdoRead_Access
, this function block is for reading all EtherCAT slave parameters.
There is an additional input, byChannelPriority
(BYTE
), with which the channel and priority can be specified in the CoE mailbox message. The first 6 bits specify the channel, the final 2 bits the priority.
See also