Dialog 'Configure Tags and Items'

Function: The dialog is for the management of the identifiers in a tree view. The assigned elements are listed underneath an identifier. User-defined identifiers can be created and their assignment to the visualization elements edited. The name of the identifier appears in the ToolBox view as a label on the button for opening the element selection.

Call: Click on symbol in the view Tools

See also

Tree view

Tags

Tree view

  • <Name>: preset identifier

  • <Name>: user-defined identifier

    Example: Favorite

Lists the assigned visualization elements. A selected visualization element can be removed by clicking on Del.

Hint: the assignment is created in the view ToolBox with the help of the context menu of a selected element.

Active

: a button for the identifier is visible in the ToolBox view.

Toolbar

The dialog Add Tag opens.

or Del

The tag selected in the tree view is removed. If you close the dialog with OK, the button is also removed from the view ToolBox.

Dialog 'Add Tag

Call: Click on the symbol in the dialog Configure Tags and Items

Name

Name of the tag

Example: tagA

Description

Example: Tagged with A