Programming a Project

This help chapter contains topics that describe all necessary steps and procedures for programming a project.

You will learn how to:

After having edited the project, continue with

NOTE:

Term definition: Standard = non-safety-related.

The term "standard" always refers to non-safety-related items/objects. Examples: a standard process data item is only read/written by a non-safety-related I/O device, i.e., a standard device. Standard variables/functions/FBs are non-safety-related data. The term "standard controller" designates the non-safety-related controller.

NOTE:

Machine Expert – Safety provides a certification manager for certifying the completed project after successful commissioning. A certified project is protected by password against modifications. (Such modifications would result in a new project acceptance procedure and certification.)

If you can't edit the project although you are logged-on correctly, verify whether the project is already certified. This is indicated in the status bar (rightmost):

Refer to the topic "Project certification" for detailed information.