Symbol:
Function: The dialog Background opens. You can define here whether the background of the visualization is colored or displayed with an image.
Call: Menu Visualization , context menu
See also
Designing a Background
Dialog 'Background'
Use Color
: Background in color
Color defined as a style color or as a fixed value.
Use Image
: Display of a background image
Reference to an image from an image pool in the project, formally specified as an instance path: <Name of the image pool>.<ID>
<Name of the image pool>.<ID>
Example:
ImagePool_A.Factory
ImagePool_B.ID_B