You can design the background of your visualization in color or with an image. To do this, use the command
.See also
In addition, you can use the property Integrate background in the dialog Properties of a visualization object to specify whether the background image should always be displayed in its entirety or whether it should be truncated.
Requirement: A project with a visualization is open.
Open the visualization and select the command
.Activate the option Image and open the input assistant.
Select an image in the dialog Input Assistant.
⇒ The image serves as a background image.
See also