IActionController.ControlCyclicAction (METH)

METHOD ControlCyclicAction

An action controller is used whenever it is necessary to have the actions of the action controller instead of those of the action provider called. ControlCyclicAction is the action controller specifically used to control the STATE.EXECUTING state.

InOut:

Scope

Name

Type

Input

itfCyclicActionProvider

ICyclicActionProvider

itfTimingController

ITimingController

Output

xComplete

BOOL

iErrorID

INT