FUNCTION_BLOCK Reconfigure EXTENDS CBM.ETrig
This function block reads and applies the whole configuration of the corresponding device and all subdevices. After Reconfiguring all changed configuration values (Enable flag, Parameter changes, ...) take effect. If device doesn't support reconfiguring eError returns ERROR.NOT_SUPPORTED.
Example
Following example code disables a slave device beneath a fieldbus master.
PROGRAM PLC_PRG
VAR
iState : INT := 0;
reconfig : DED.Reconfigure;
END_VAR
CASE iState OF
0: //Disable slave device: Slave1 (= name in device tree)
Slave1.Enable := FALSE;
iState := 1;
1: //start reconfiguring of fieldbus master
reconfig(xExecute := TRUE, itfNode := Master);
IF reconfig.xDone THEN
iState := 3;
ELSE IF reconfig.xError THEN
iState := 2;
END_IF
2: //reconfiguring error
//TODO: Add code here
reconfig(xExecute := FALSE);
3: //reconfiguring successful ==> slave disabled
//TODO: Add code here
reconfig(xExecute := FALSE);
END_CASE
This feature may not be supported by all fieldbus drivers. eError will return ERROR.NOT_SUPPORTED if not supported.
| InOut: |