FUNCTION_BLOCK Open EXTENDS CBM.ETrig
Open a serial com port.
The input Parameters are a list of settings, with which the COM port should be opened.
MyComOpen : COM.Open;
aParamsB115200 : ARRAY [1..7] OF COM.PARAMETER := [
(udiParameterId := COM.CAA_Parameter_Constants.udiPort, udiValue := 1),
(udiParameterId := COM.CAA_Parameter_Constants.udiBaudrate, udiValue := 115200),
(udiParameterId := COM.CAA_Parameter_Constants.udiParity, udiValue := COM.PARITY.NONE),
(udiParameterId := COM.CAA_Parameter_Constants.udiStopBits, udiValue := COM.STOPBIT.ONESTOPBIT),
(udiParameterId := COM.CAA_Parameter_Constants.udiTimeout, udiValue := 0),
(udiParameterId := COM.CAA_Parameter_Constants.udiByteSize, udiValue := 8),
(udiParameterId := COM.CAA_Parameter_Constants.udiBinary, udiValue := 1)
];
IMPLEMENTATION:
So to parameterize the FB looks like:
MyComOpen(usiListLength := SIZEOF(aParamsB115200)/SIZEOF(COM.PARAMETER), pParameterList := ADR(aParamsB115200));
...
InOut: |
|