The SF_EmergencyStop function block monitors the switching states of an emergency-stop control device and executes stop category 0 at its output. S_StartReset and S_AutoReset can be used to specify a start-up inhibit and a restart inhibit.
When the connected emergency-stop control device is activated, the function block ensures that the enable signal at the S_EStopOut output switches to SAFEFALSE. The process being controlled is stopped.
S_StartReset is used to specify the start-up inhibit after activating the function block and/or starting the Safety Logic Controller.
S_StartReset = SAFEFALSE |
After the Safety Logic Controller has been started up and/or the function block has been activated at input Activate, the start-up inhibit is active. The start-up inhibit is only removed if there is a positive signal edge at the Reset input. Refer to the hazard message below this table. |
S_StartReset = SAFETRUE |
After the Safety Logic Controller has been started up and/or the function block has been activated at input Activate, no start-up inhibit is active. Refer to the section "Attention when using ...". |
Removing the start-up inhibit by means of a positive signal edge at the Reset input can cause the S_EStopOut output to switch to SAFETRUE immediately (depending on the status of the other inputs).
WARNING | |
---|---|
S_AutoReset specifies a restart inhibit after the connected emergency-stop control device has been deactivated.
S_AutoReset = SAFEFALSE |
After the connected emergency-stop control device has been deactivated, the restart inhibit is active. The restart inhibit is only removed if there is a positive signal edge at the Reset input. After the restart inhibit has been removed, the status at the S_EStopOut output can switch from SAFEFALSE to SAFETRUE. Refer to the hazard message below this table. |
S_AutoReset = SAFETRUE |
The restart inhibit is not specified. As soon as the emergency-stop control device is deactivated and the SAFETRUE value is present at the S_EStopIn input again, the S_EStopOut output switches to SAFETRUE automatically. Refer to the section "Attention when using ...". |
Removing the restart inhibit by means of a positive signal edge at the Reset input can cause the S_EStopOut output to switch to SAFETRUE immediately (depending on the status of the other inputs).
WARNING | |
---|---|
The start-up inhibit and/or restart inhibit must only be deactivated if it is certain that starting up/restarting the machine/system will not lead to a hazardous situation or that a suitable start-up/restart inhibit is in place at another location or using other means.
WARNING | |
---|---|