FUNCTION_BLOCK SMC_CalcDirectionFromVector
By use of this function the orientation (dAlpha) of the tool can be calculated.
Note
For detailed information on transformation function blocks see the survey on SM_Trafo_POUs.
|
InOut:
|
|
Scope
|
Name
|
Type
|
Initial
|
Comment
|
|
Input
|
v
|
SMC_VECTOR3D
|
|
Tangent vector v. In general, v will be identical to the output vecActTangent of the interpolator.
|
|
eDir
|
SMC_VECTORDIR
|
SMC_tangential
|
Input eDir specifies, whether the direction has to be calculated parallel to a path tangent (SMC_tangential), or oppositely (SMC_opp_tangential) or orthogonally to the path (SMC_orthogonal_r (right to the path tangent) resp. SMC_orthogonal_l (left to the path tangent)).
|
|
Output
|
dDir
|
LREAL
|
|
The angle dDir is measured in degrees. It will remain constant during standstill of the interpolator, i.e. when v is the zero vector. eDir is mostly either used as set value at
|SMC_ControlAxisByPos| for a directional axis or as input dAlpha for the transformation.
|
|