SMC_VECTORDIR (ENUM)

TYPE SMC_VECTORDIR :

This enumeration variable is used as an input variable at SMC_CalcDirectionFromVector to define if the angle of the vector itself, its inverse or one of the two perpendiculars shall be used.

InOut:

Name

Initial

Comment

SMC_tangential

0

No offset; tangential direction

SMC_orthogonal_r

-90

Offset -90; orthogonal direction clockwise

SMC_orthogonal_l

90

Offset 90; orthogonal direction counterclockwise

SMC_opp_tangential

180

Offset 180; opposite direction

Input eDir indcates, whether the direction is calculated parallel to the path tangent (MC_tangential), opponent (SMC_opp_tangent) or orthogonal (SMC_orthogonal_r = right of the path tangent, SMC_orthogonal_l = left of the path tangent).