Function: This command loads an ASCII
file with CNC program data into the CNC editor. The CNC object retains its name.
Call: Menu bar:
.Requirement: A CNC object is open in the editor.
The command opens the default dialog box for searching the file system. The filter must be set to CNC, GCODE, or TXT. The selected file is loaded into the active CNC editor. Any existing CNC program is overwritten (after another query).
See also