Command 'Write program to ASCII file'

Function: This command opens the standard dialog box for saving a file in the file system. The CNC program can be saved as an ASCII file.

Call: Menu bar: CNC .

Requirement: A CNC path is open in the editor.

Name

Preset: Name of the CNC object

Example: cncSpiral_A

File type

File extension: TXT, GCODE, CNC

See also