Command 'CommitAllChanges'

Function: This command commits all changes of the CODESYS project to the SVN repository.

Call: Action in the Test Manager TestManager.SVN

Requirement: The CODESYS Test Manager add-on is installed.

Configuration

Commit Message

The log message for the commit.

Commit Options

Keep locks

: The locks are not removed after the commit.

Keep change lists:

: The change list is not removed after the commit.

Update after commit (recommended):

: The project is updated after the commit and prevents mixed revisions in the working copy. (For more information, refer the svnbook homepage.)

See also