Function: This dialog defines the permissions of user groups for a visualization element.
Call: Click in the Value field of the Access Rights element property of a visualization element.
Requirement: A visualization element is selected in a visualization element and the Properties is open.
User Groups |
Groups that were configured in the Visualization Manager (tab ). |
Operable |
|
Only Visible |
|
Invisible |
|
Group hierarchy is used |
Display whether the option Use group hierarchy is activated in the Visualization Manager (tab ). A group of a higher hierarchy cannot have fewer permissions for an element than an element of a lower hierarchy. |
If no user is logged in, then the permissions apply for the visualization elements that are configured for the user group None. If the permissions for a visualization element is restricted, then the group None should be granted the lowest permissions.
See also