Function: This dialog box is part of the wizard that opens when you create a new project with the HMI project template. This allows for adding usual objects conveniently.
Call: Automatically after the Create HMI Project - Connect to HMI Device dialog box
See also
alarm configuration |
|
Image pool |
|
Recipe manager |
|
Text list |
|
Unit conversion |
|
Trend recording manager |
|
Program |
|
Next > |
The selection is accepted and the Create HMI Project - Select Perspective dialog box opens. |
Abort |
The configuration and settings of an HMI project are ended. |
See also