Symbol:
Function: The options define the use of visualization user management for global visualizations in the POUs view and for visualizations that are linked from libraries.
Call: Menu bar: Tools.
Requirement: A visualization user management exists.
Do not use visualization user management |
The affected visualizations behave as when no user management is configured. |
Use the following visualization user group list |
|
Derive visualization user management automatically |
The affected visualizations use the user management configuration of the visualization manager selected here. The drop-down list shows all visualization managers of the project. If this is not possible, then the user groups are used from the option Use the following user group list for the visualization. |
The user management for a visualization in the Devices view is configured in the Visualization Manager (tab User Management).
See also