Visualization Element 'Spin Box'

Element properties

Element name

Example: Speed controller conveyor belt

Optional

Hint: Assign individual names for elements so that they are found faster in the element list.

Type of element

Spin Box

Element property 'Position'

The position defines the location and size of the element in the visualization window. These are based on the Cartesian coordinate system. The origin is located at the upper left corner of the window. The positive horizontal x-axis runs to the right. The positive vertical y-axis runs downwards.

X

X coordinate of the upper left corner of the element

Specified in pixels.

Example: 10.

Y

Y coordinate of the upper left corner of the element

Specified in pixels.

Example: 10.

Width

Specified in pixels.

Example: 150

Height

Specified in pixels.

Example: 30

Note

You can also change the values by dragging the box symbols () to other positions in the editor.

See also

Element property 'Center'

The properties contain fixed values for the coordinates of the point of rotation. This point of rotation is shown as the symbol. The point is used as the center for rotating and scaling.

X

X-coordinate of the point of rotation

Y

Y-coordinate of the point of rotation

Note

You can also change the values by dragging the symbols () to other positions in the editor.

Variable

Variable (numeric data type)

Example: PLC_PRG.iTemp

Number format

Format of the value in printf syntax

Example: %d, %5.2f

Interval

Interval used for modification of the value

Element property 'Value range'

Minimum value

Lower limit of the output value

  • fixed value

  • Variable (INT)

Maximum value

Upper limit of the output value

  • fixed value

  • Variable (INT)

Element property 'Text properties'

The properties contain fixed values for the text properties.

Usage of

  • Default style values: The values of the visualization style are used.

  • Individual settings: The "Individual text properties" property group is shown The values can be customized here.

Individual text properties

Requirement: The Individual settings text property is defined.

Horizontal alignment

Horizontal alignment of the text within the element.

Vertical alignment

Vertical alignment of the text within the element.

Font

Example: Default

: The Font dialog box opens.

: Drop-down list with style fonts.

Font color

Example: Black

: The Color dialog box opens.

: Drop-down list with style colors.

Transparency

Whole number (value range from 0 to 255). This determines the transparency of the respective color.

Example: 255: The color is opaque.

0: The color is completely transparent.

Please note: If the color is a style color and already has a transparency value, then this property is write-protected.

Element property 'Color variables'

The Element property is used as an interface for project variables to dynamically control colors at runtime.

Toggle color

The property controls the toggled color at runtime.

Value assignment:

  • FALSE: The element is displayed with the color specified in the Color property.

  • TRUE: The element is displayed with the color specified in the Alarm color property.

Assigning the property:

  • Placeholder for the user input variable

    • <toggle/tap variable>

    • <NOT toggle/tap variable>

    The color change is not controlled by its own variable, but by a user input variable.

    Note: Specify a variable for the mouse events Tap or Toggle in the input configuration of the element. Only then is the placeholder set. If you configure a variable in both Toggle and Tap, then the variable specified in Tap is used.

    Hint: Click the symbol to insert the placeholder <toggle/tap variable>. When you activate the Inputconfiguration, Tap FALSE property, then the <NOT toggle/tap variable> placeholder is displayed.

  • Instance path of a project variable (BOOL)

    Example: PLC_PRG.xColorIsToggeled

    Note: In the code, declare and implement the variable specified here. Its value assignment determines when the color changes.

Note

The transparency part of the color value is evaluated only if the Activate semi-transparent drawing option of the visualization manager is selected.

Note

Select the Advanced option in the toolbar of the properties view. Then all element properties are visible.

See also

Element property 'Absolute movement'

The properties contain IEC variables for controlling the position of the element dynamically. The reference point is the upper left corner of the element. In runtime mode, the entire element is moved.

Movement

X

Variable (numeric data type). Defines the X position (in pixels).

Example: PLC_PRG.iPos_X.

Increasing this value in runtime mode moves the element to the right.

Y

Variable (numeric data type). Defines the Y position (in pixels).

Example: PLC_PRG.iPos_Y.

Increasing this value in runtime mode moves the element downwards.

Rotation

Variable (numeric data type). Defines the angle of rotation (in degrees).

Example: PLC_PRG.iAngle1.

The midpoint of the element rotates at the Center point. This rotation point is shown as the symbol.

In runtime mode, the alignment of the element remains the same with respect to the coordinate system of the visualization. Increasing the value rotates the element to the right.

Interior rotation

Variable (numeric data type). Defines the angle of rotation (in degrees).

Example: PLC_PRG.iAngle2.

In runtime mode, the element rotates about the point of rotation specified in Center according to the value of the variable. In addition, the alignment of the element rotates according to the coordinate system of the visualization. Increasing the value in the code rotates clockwise.

The rotation point is shown as the symbol.

Note: If a static angle of rotation is specified in the Position ‣ Angle property, then the static angle of rotation is added to the variable angle of rotation (offset) when the visualization is executed.

Note

You can link the variables to a unit conversion.

Note

The X, Y, Rotation, and Interior rotation properties are supported by the "Client Animation" functionality.

See also

Element property 'State variables'

The variables control the element behavior dynamically.

Invisible

Variable (BOOL). Toggles the visibility of the element.

TRUE: The element is not visible at runtime.

Example: bIsVisible with VAR bIsVisible : BOOL := FALSE; END_VAR

Deactivate inputs

Variable (BOOL). Toggles the operability of the element.

TRUE: User inputs do not have any effect in runtime more. The element is shown as deactivated.

Note

The Invisible property is supported by the "Client Animation" functionality.

See also

These properties are available only when you have selected the Preview: Support client animations and overlay of native elements option in the Visualization Manager.

Animation duration

Defines the duration (in milliseconds) in which the element runs an animation

  • Variable (integer value)

    Example: Menu.tContent with VAR tContent : INT := 500; END_VAR

  • Integer literal

    Example: 500

Animatable properties

  • Absolute movement, Movement, X, Y

  • Absolute movement, Rotation

  • Absolute movement, Interior rotation

  • Absolute movement, Exterior rotation

The animated movement is executed when at least one value of an animatable property has changed. The movement then executed is not jerky, but is smooth within the specified animation duration. The visualization element travels to the specified position while rotating dynamically. The transitions are smooth.

Move to foreground

Moves the visualization element to the foreground

Variable (BOOL)

Example: bIsInForeground with VAR bIsInForeground : BOOL := FALSE; END_VAR

TRUE: At runtime, the visualization element is displayed in the foreground.

FALSE: At runtime, the visualization element is displayed in the layer where it was inserted in the visualization editor.

See also

Element property 'Input configuration'

The properties contain the configurations for the user input when using the mouse or keyboard. User input is a user event from the perspective of the element.

Note

The input configuration refers to the text area of the element only, not the two buttons.

The Configure button opens the Input configuration dialog box for creating or modifying a user input configuration.

A configuration contains one or more input actions for the respective input event. Existing input actions are displayed below it.

Example: Execute ST code: PLC_PRG.i_x := 0;

OnDialogClosed

Input event: The user closes the dialog box.

OnMouseClick

Input event: The user clicks the element completely. The mouse button is clicked and released.

OnMouseDown

Input event: The user clicks down on the element only.

OnMouseEnter

Input event: The user drags the mouse pointer to the element.

OnMouseLeave

Input event: The user drags the mouse pointer away from the element.

OnMouseMove

Input event: The user moves the mouse pointer over the element area.

OnMouseUp

Input event: The user releases the mouse button over the element area.

See also

Tap

When a mouse click event occurs, the variable defined in Variable is described in the application. The coding depends on the options Tap FALSE and Tap on enter if captured.

Variable

Variable (BOOL). Contains the information whether a mouse click event exists.

Example: PLC_PRG.bIsTapped

TRUE: A mouse click event exists. It lasts while the user presses the mouse button over the element. It ends when the button is released.

FALSE: A mouse click event does not exist.

Requirement: The Tap FALSE option is not activated.

Tap FALSE

: The mouse click event leads to a complementary value in Variable.

TRUE: A mouse click event does not exist.

FALSE: While the mouse click event exists.

Tap on enter if captured

: During user input, it is also taken into consideration whether the mouse pointer is dragged within the element area or not while the mouse button is pressed.

TRUE: While the mouse click event exists and the mouse pointer is moved over the element area.

FALSE: A mouse click event does not exist. Or the user moves the mouse pointer outside of the element area while the mouse button is pressed.

The value is TRUE again as soon as the user moves the pointer back to the element area. The mouse is then captured.

Shift

When a mouse click event occurs, the variable here is described in the application. When the mouse click event ends, its value is toggled with the Toggle on up if captured option.

Variable

Variable (BOOL). Its value toggled when the mouse click event is ended. This is when the user releases the mouse button while the mouse pointer is over the element area.

If the user releases the mouse button while the mouse pointer is outside of the element area, then the mouse click event is not ended and the value is not toggled.

Tip: The user can cancel a started toggle input by dragging the mouse pointer out of the element area.

Toggle on up if captured

: The value toggles regardless of where the mouse pointer is when the mouse button is released. The mouse is then captured.

Hotkeys

Keyboard shortcut on the element for triggering specific input actions.

When the keyboard shortcut event occurs, the input actions in the Event(s) property are triggered. In this way, it is not the input action itself that leads to this input action, but the mouse input action.

Key

Key pressed for input action.

Example: T

Note: The following properties appear when a key is selected.

Event(s)

  • None

  • Mouse down: Pressing the key triggers the input actions that are configured in the OnMouseDown property.

  • Mouse up: Releasing the key triggers the input actions that are configured in the OnMouseUp property.

  • Mouse down/up: Pressing and releasing the key triggers the input actions that are configured in the OnMouseDown property and the OnMouseUp property.

Shift

: Combination with the Shift key

Example: Shift+T.

Control

: Combination with the Ctrl key

Example: Ctrl+T.

Alt

: Combination with the Alt key

Example: Alt+T.

Note

All keyboard shortcuts and their actions that are configured in the visualization are listed in the Keyboard configuration tab.

See also

Element property 'Access rights'

Requirement: User management is set up for the visualization.

Access rights

Opens the Access rights dialog. There you can edit the access privileges for the element.

Status messages:

  • Not set. Full rights.: Access rights for all user groups : operable

  • Rights are set: Limited rights: Access is restricted for at least one group.

See also

See also