Symbol:
The object represents a single visualization. You can insert a visualization under an application or, so that it is available project-wide, under the root node of the view Devices or directly in the view POUs. You can open the visualization editor for editing by double-clicking on the object entry in the device tree or in the view POUs.
See also