SMC_Trafo_Tripod_Lin (FB)

FUNCTION_BLOCK SMC_Trafo_Tripod_Lin

Inverse transformation for tripod

InOut:

Scope

Name

Type

Initial

Comment

Input

pi

SMC_PosInfo

Position of the inner ring’s center (x,y,z)

dOuterRadius

LREAL

Radius of outer ring

dInnerRadius

LREAL

Radius of inner ring

dLength

LREAL

Length of linkage

dDistance

LREAL

Distance between two cooperating linkages

dRotationOffset

LREAL

0

Angle of axis A

dAxisAngle

LREAL

Absolute angle between rails and z-axis

dSingularityTolerance

LREAL

1

dOffsetA

LREAL

Offset that is subtracted from the resulting position of drive A.

dOffsetB

LREAL

Offset that is subtracted from the resulting position of drive B.

dOffsetC

LREAL

Offset that is subtracted from the resulting position of drive C.

Output

dLA

LREAL

Resulting position of drive A. The 0 position is at the point where the axis, along which the drive moves, intersects the plane where the dOuterRadius is measured. Can be adjusted by dOffsetA.

dLB

LREAL

Resulting position of drive B. The 0 position is at the point where the axis, along which the drive moves, intersects the plane where the dOuterRadius is measured. Can be adjusted by dOffsetB.

dLC

LREAL

Resulting position of drive C. The 0 position is at the point where the axis, along which the drive moves, intersects the plane where the dOuterRadius is measured. Can be adjusted by dOffsetC.

bError

BOOL

Only TRUE, if there is no solution

bSingularPosition

BOOL

At least one drive is near a singular position

bNegativeDrivePosition

BOOL

At least one drive’s position is calculated to be negative