System
FloatingPointUtils
3.5.17.0
Intern|Utils
FPU
None
Helper functions for REAL and LREAL numbers.
ESpecial_FP_Value (Enum)
Functions
Ceil (Function)
CeilF (Function)
Floor (Function)
FloorF (Function)
Truncate (Function)
TruncateF (Function)
HexReal
DeserializeHexReal (Function)
SerializeHexReal (Function)
LREAL
GetLRealSpecialVal (Function)
IsLRealNaN (Function)
IsLRealNegInfinity (Function)
IsLRealNumber (Function)
IsLRealPosInfinity (Function)
REAL
GetRealSpecialVal (Function)
IsRealNaN (Function)
IsRealNegInfinity (Function)
IsRealNumber (Function)
IsRealPosInfinity (Function)
StringFunctions
HexStrToLReal (Function)
HexStrToReal (Function)
LRealToHexStr (Function)
LRealToStr (Function)
RealToHexStr (Function)
RealToStr (Function)
StrToLReal (Function)
StrToReal (Function)
[1]
Based on FloatingPointUtils.library, last modified 20.04.2021, 15:17:29. LibDoc 4.0.0.0
The content file FloatingPointUtils.clean.json was generated with CODESYS V3.5 SP16 Patch 3 on 20.04.2021, 15:17:29.