SMC_Seg (STRUCT)

TYPE SMC_Seg : STRUCT

This structure is used internally by the SMC_Interpolator . It represents a path segment of fixed length in which a certain acceleration shape is used.

InOut:

Name

Type

Comment

eType

SMC_SEGMENTTYPE

The type of the segment.

dLength

LREAL

The length of the segment

dVelStart

LREAL

The start velocity of the segment (non-negative)

dVelEnd

LREAL

The end velocity of the segment (non-negative)

dAccStart

LREAL

The start acceleration (signed)

dAccEnd

LREAL

The end acceleration (signed)

dJerk

LREAL

The jerk (signed), only used for changing acceleration