CharBufferString.CopyFrom (METH)

METHOD CopyFrom

Does a strcpy from the source string cbsSource into our instance at given positions and a given length. Note: No terminating 0 will be appended.

InOut:

Scope

Name

Type

Comment

Input

rcbsSource

REFERENCE TO CharBufferString

The source string, where the characters will be copied from

diSourceOffset

DINT

The 1 relative offset within the source string, where the copying will start

diTargetOffset

DINT

The 1 relative offset within the source string, where the copying to will start

diCountCharacters

DINT

The number of characters to copy