|
Input
|
m_uiBufferSize
|
UINT
|
The size of the buffer (in bytes), where the string is stored.
|
|
m_cbpBuffer
|
CharBufferPtr
|
The buffer, where the string is stored this instance represents
|
|
m_Type
|
__SYSTEM.TYPE_CLASS
|
A __SYSTEM.TYPE_CLASS value indicating type of the string
|
|
m_AsString
|
POINTER TO STRING(255)
|
Two additional pointers to the buffer used for easier debugging. In the monitoring view the corresponding pointer shows the current value of the buffer as (w)string.
|
|
m_AsWString
|
POINTER TO WSTRING(255)
|
|
|
m_bAllocated
|
BOOL
|
Flag indicating, whether the memory for storing the string was allocated dynamically and has to be freed later
|