IETrigTlTo (ITF)

INTERFACE IETrigTlTo EXTENDS IETrigTl, ITimeOutConstraint

In order to build a function block with an ETrigTlTo behaviour, its action provider has to be decorated with this interface. This will determine the state machine which then forces the function block to the appropriate ETrigTlTo behaviour.

See Decorators for more information about the concept.

A state chart for function blocks with ETrigTlTo behaviour

Starting

StartAction is running, until xComplete is TRUE, xBusyTRUE

At its beginning the SampleAction is probably executed one time.

Executing

CyclicAction is running until xComplete is TRUE

Cleaning

CleanupAction is running. At its end the ExitAction is probably executed one time.

After a Ready Condition as input, only the output states

Done (xComplete is TRUE) or Error (eErrorIDERROR.NO_ERROR) are possible.

After a Error Condition as input, only the output state

Error (eErrorIDERROR.NO_ERROR) is possible.

Done

xDoneTRUE, xBusyFALSE

Error

xErrorTRUE, eErrorIDERROR.NO_ERROR, xBusyFALSE

Resetting

ResetAction is running, until xComplete is TRUE.

After that:

- the outputs xDone and xError will be set to FALSE.

- The output eErrorID will be set to ERROR.NO_ERROR.

Methods:

StartAction, inherited from IStartActionProvider