FUNCTION_BLOCK LCon EXTENDS BehaviourModelBase IMPLEMENTS ILCon
Base implementation of a PLCopen Level Controlled Behavior Model (see: ILCon)
For use, this block should be extended and the specific inputs and outputs must be supplemented. The output eErrorID of the application-specific enum type ERROR must be added.
InOut: |
|
Properties:
ActionController, inherited from BehaviourModelBase
ModelTimeLimit, inherited from BehaviourModelBase
ModelTimeOut, inherited from BehaviourModelBase
Methods:
CleanupAction, inherited from BehaviourModelBase
CyclicAction, inherited from BehaviourModelBase
ExitAction, inherited from BehaviourModelBase
GetConfiguration, inherited from BehaviourModelBase
GetConfiguration2, inherited from BehaviourModelBase
ResetAction, inherited from BehaviourModelBase
StartAction, inherited from BehaviourModelBase
Structure: