Opening a meter security configuration file
Meter security settings are stored in an encrypted Security Configuration File (SCF).
Use ION Setup to open an SCF file.
Prerequisites:
- Meter connection using ION Setup.
 - Device credentials.
 - Security configuration access.
 
To open the meter security configuration file:
- In ION Setup, open the Setup Assistant for your meter.
 - Select Security > Security Mode > Edit.
 - If prompted, enter the meter password, and then select OK.
 - 
                                                
Select the SCF file that you want to edit, and then select Open.
The Select security mode screen appears.
 - Select the Password Complexity. 
Tip: For more information on the enforcement rules for each option, hover over the drop-down.
 - Enter the Minimum Password Length. 
Note: The Minimum Password Length can be up to 16 characters and must be 6 characters or greater if Password Complexity is set to IEEE 1686-2013 or NERC CIP-007-5.
 - 
                                                
Select Next.
 
The meter security configuration settings open in the ION Setup Security wizard.
Next, configure the meter security settings.
Related topics: