Modifying roles

Conditions préalables :

Use CAE to modify the roles in a project.

You can:

Creating a role

To create a role:

  1. Select Roles.

  2. Select Create a New Role.

    Conseil : To create a new role based off an existing role, select a role and then select Duplicate Role.

  3. Enter the Role Details details.

  4. Select Save.

  5. Select the Associated Models and Permissions.

    Pour plus d’informations on the available permissions, see Roles and Permissions.

Editing a role

To edit a role:

  1. Select Roles.

  2. Select the role that you want to edit.

  3. (Facultatif) Enter the Role Details details.

  4. (Facultatif) Select the Associated Models and Permissions.

    Pour plus d’informations on the available permissions, see Roles and Permissions.

Deleting a role

To delete a role:

  1. Select Roles.

  2. Select the role that you want to delete.

  3. Select Delete Role.

  4. Select the Yes to confirm the deletion.